Other Parts Discussed in Thread: ADS124S08, ADS1248
The ADS131M06 has multiple ADCs and thus consumes more power than the ADS1248 and ADS124S08 ICs that use multiplexers, but the advantage is that it can acquire inter-channel data outputs simultaneously, which allows a shorter time to acquire synchronized data across all channels. We are interested in adopting this IC.
I would like to know if the noise level is the same or better than the above ICs when set in the same bandwidth.
What is the input referred noise value on the low frequency side when using the internal digital filter of the ADS131M06?
The datasheet "Table 7-1. Noise at TA = 25° (μVRMS)" only gives data up to 250 Hz. please tell me the noise at ODR = 1 Hz / 5 Hz / 10 Hz. The gains used are around 32 / 64 /128.
ADS131M06 noise ADC ADS1248 ADS124S08 syncronized data