Other Parts Discussed in Thread: ADC32RF44, ADC32RF54, ADS54J66, ADC32RF42
Hi team
1. Is ADC12DJ800 capable of measuring near DC frequency signal? From the datasheet 8.4.6 it says that near DC signal is not allowed with Background Calibration enabled.
2. If measuring DC frequency signal is possible as long as Background Calibration is disabled, could you please advise according to below:
2-1) Necessary time to perform Foreground Calibration
2-2) Offset drift by time (datasheet has VOFF_DRIFT but this is temperature drift correct?)
3. Does ADC12DJ800 have Interleave Spurs between ADC cores? Or is it removed by Background Calibration?
My customer is currently using ADC32RF44 and had some Interleave Spurs came out from the offset error between ADC cores, but it can be removed through the Fs/8・Fs/4・Fs*3/8・Fs/2 offset corrector.
I don't see this function on the datasheet of ADC12DJ800
4. Could you please advise a better solutions if ADC12DJ800 does not seem to be the best one?
Regards