Do VCC supply need a LDO for a stable output ? Can a DC-DC regulator supply VCC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Do VCC supply need a LDO for a stable output ? Can a DC-DC regulator supply VCC?
Hello,
An LDO would be the recommended supply for a stable output. Any switching noise from a DCDC regulator will appear on the analog outputs.
Best,
Katlynne Jones
Why? I think ,the switching noise will not appear on the output directly, it will be suppressed by PSRR of output amplifier. ok?
Hi,
It depends on the PSRR of the output amplifier and the frequency of the DCDC. Generally, our devices have limited bandwidth, so noise over ~500kHz should probably be filter externally. We generally do not see better than -60dB PSRR, so it depends on the magnitude of the supply ripple. If you know the switching frequency, you can use some techniques to filter just that. You could improve noise performance by adding more discrete capacitors or series resistors on the supply pins to help attenuate the noise.
Thanks,
Paul