Other Parts Discussed in Thread: ADS8681EVM-PDK, ADS7142, ADS8681
I configured the ALARM/SDO-1/GPO pin as an alarm by setting SDO_CTL_REG bits 9-8 to 01b per table 7-14 (SDO_CTL_REG Register Field Descriptions).
I would like the GPIO pin to function as an active alarm for the alarm input and go low or high based on an active alarm condition. Unfortunately, it is functioning as a tripped alarm. It goes high upon an alarm condition but does not go low when the alarm condition is over. Instead, you have to read the ALARM_REG register to clear the GPIO pin low.
Is there any way to make the ALARM/SDO-1/GPO pin function as an active alarm instead of a tripped alarm?