Other Parts Discussed in Thread: ADS7128
Dear Sir, please answer
I need to measure “average voltage value” - let's call it like that, because this value cannot be called RMS.
I have signal source, figure 1. Signal frequency – 50 Hz. I feed it to operational amplifier rectifier and have signal figure 2. I feed then it to operational amplifier integrator and have signal figure 3. (amplifiers are powered by plus 5 V and minus 5V). I feed signal to ADC then. ADC has 5V reference.
I need now to use +5V power only, and I have +2.5 V reference (or +5 V) for ADC operation.
I can generate the following signal using operational amplifier – figure 4.
QUESTION: how can I use ADC like ADS7951 in order to get as a result something like, what I got before?
I understand this: do I need to take signal samples at intervals of about 0.1 - 0.2 ms and then calculate the average value?
What ADC circuit to apply?
Please, see figures 1 - 4 in attach.
TIA
Sincerely,
Vladimir Naumenkov