Part Number: ADS9817EVM-PDK
I was looking at the ADS9817EVM-PDK evaluation board and the datasheet specifies that there should be a GUI that comes with it to both set the configuration registers of the ADC and program an FPGA connected to the board. Section 5 of the datasheet mentions that there should be a "Tools and Software" folder but I have not seen it. If I could be pointed to where the GUI is it would be appreciated. I would also like to know if the code for the GUI and the FPGA is open source so that it could be modified.