This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am interested in identify the clinical-grade pulse oximetry AFEs.
When filtering the product catalog, I see that four options are viable: AFE4404, AFE4403, AFE4400, and AFE4490
But looking at the Bio-Sensing AFE chart, I noticed that AFE4404 is not labeled as a medical AFE
So should the AFE4404 be used for medical-grade applications? Or is more suited for home-monitoring purposes?
Also, what would be the main differences between the AFE4403 and AFE4404? I suspected the AFE4404 is an up-revision to the AFE4403 but it seems that is not the case.
Hi,
Most of these discussions are under NDA. I will reach out to you via email.