This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi.
I am doing PPG test using AFE4404.
I was watching Chip Applications, and I got a question, so I'm asking.
Check out the AFE4404 chip applications.
It says so.
Some chips are written the same way, but others are written differently. Ex. AFE4432
Does Clinical finger tip pulse oximetry and SPO2 mean different things?
Does that mean that AFE4404 is not suitable for measuring SPO2 on the wrist?
Or it can be measured on the wrist, but does it mean that the fingers come out better?
Thank you.
Hi,
It's highly suggested/recommended to do some study about the PPG, SpO2, Clinical finger tip pulse oximetry.
SpO2 is a high level(super set) term for (S)aturation (O2)xygen particular in (p)eripheral, where peripheral could be/mean any peripheral depending on people's definition/usage as long as it's not directly into the blood, not around the heart region/area.
"
Peripheral oxygen saturation (SpO2) is an estimation of the oxygen saturation level usually measured with a pulse oximeter device. It can be calculated with pulse oximetry
Pulse oximetry is a method used to estimate the percentage of oxygen bound to hemoglobin in the blood.This approximation to SaO2 is designated SpO2 (peripheral oxygen saturation). The pulse oximeter consists of a small device that clips to the body (typically a finger, an earlobe or an infant's foot) and transfers its readings to a reading meter by wire or wirelessly. The device uses light-emitting diodes of different colours in conjunction with a light-sensitive sensor to measure the absorption of red and infrared light in the extremity. The difference in absorption between oxygenated and deoxygenated hemoglobin makes the calculation possible.
"
Regarding to "Does that mean that AFE4404 is not suitable for measuring SPO2 on the wrist?" -
Whether it can be used on the which peripheral parts/areas and the related performance, it depends on customer's products designs(particular opticals, mechanical opticals and algorithms, etc), not really related to the chip.
Regarding to "Or it can be measured on the wrist, but does it mean that the fingers come out better?"-
Overall and/or in general, finger tips with transmitted optical approaches may yield better results.
----------------------------------
It's highly suggested/recommended to do some basic study and research to understand the PPG, SpO2, pulse oximeter in different approaches.
Thanks
Thank you for your reply.
Peripheral oxygen saturation (SpO2) is an estimation of the oxygen saturation level usually measured with a pulse oximeter device. It can be calculated with pulse oximetry
I mean, I can get Peripheral Oxygen saturation (SpO2) with pulse oximetry, but why did you divide it up in chip applications?
Ex. AFE4404 applications - fingertip pulse oximetry, AFE4432 applications - SPO2
Thank you.
Hi,
There is no divide.
It depends on how people want to interpret.
finger tip pulse oximetry. developers/designers should know what pulse oximetry is, and it can be used to measure SpO2.
SpO2. developers/designers should know what SpO2 is, and and it could be measured by PPG method using Pulse Oximeter.
Thanks