Hi,
I am using ADS54j66 ADC. I have an requirement multi chip synchronization. it was achieved by JESD204b subclass 1.
two adc's are mounted in the board.
Following are JESD204B parameters.
No of lanes L = 4
No of convertors M = 4
Octets per frame F = 2
Frames per multiframe K = 16
Samples per frame S = 1
Sampling clock = 300Mhz
Frame clock = 300Mhz
To find the LMFC boundary of ADS54j66, i intentionally added the delay in one of the Convertor SYNC pin.
when ever sync pin delay across the ADC exceeding one LMFC boundary, i was expecting 16(Frames per multi frame) frame clock delay in ILA sequence.
But it was observed 32 frame clock delay in ILA Sequence across the ADC.
when LMFC count in the ADC(ADS54J66) will wrap to zero ? If it is Frames per multi frame i should get 16 frame clocks delay in ILA.
Kindly clarify.
Thanks in advance.
Regards,
Sarojini