Hi team,
According to the datasheet, 7.3.4 Digital Output, it seems that the digital output code correspoding to the input voltage can follow as below. Is this undertanding correct?
When the differential input is +250mV, digital output code will be 58368.
When the differential input is -250mV, digital output code will be 7168.
So this means that the peak-to-peak voltage is -250mV to +250mV and the code of the peak-to-peak voltage is 58368 - 7168 = 51200.
This means the amplitude is +250mV, the code range of amplitude is 51200/2 = 25600.
Therefore, when the differentail input is +150mV, digital output code will be 25600*150mV/250mV = about 15360.
Regards,
Noriyuki Takahashi