Hi! We are students working on a master thesis project involving sending and reading analog data. We have been looking for a combined DAC/ADC module with requirements:
16 channel analog output
6 channel analog input
Resolution: 12 bits, preferably 16 or more
Sampling rate: 1kHz or more
Input voltage tolerance: 0-3.3V or more
USB and serial UART interfaces
Have a UI (user interface)
Possibility to output recordings of data (.mat files)
So far the best device option we have is the AMC7836, which fulfills all requirements except for the UART interface. We need this to be able to read in an analog signal from another device that only communicates with UART. Do you have any converters/adapters that could read UART and convert it to SPI which the AMC7836 can read? OR do you maybe have other devices available that fulfill all of our requirements?