This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC53004: Under-shoot on VOUT while setting output voltage

Part Number: DAC53004

Hello,

I am using the DAC53004 to limit the current in a H-Bridge. The VOUT of the DAC (OUTA and OUTB) are connected to the gates of the MOSFETs and the FB (FBA and FBB) are connected to the sources.

I measured the differential voltage between E1 and E2 and I observed an "under-shoot". The red arrow is when the OUT of the DAC are enabled.

To see if the problem was coming from my circuit or from the DAC, I removed the DAC from the circuit and I connected OUT to FB directly.

This is the result:

Any reason why the DAC would do that?

Thanks for your help.

Best Regards