This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7952-Q1: ADS7952-Q1 Issue

Part Number: ADS7952-Q1

Dear Sir:

Regarding the ADS7952-Q1 Issue.

1. MULTIPLEXER :CH0~ CH11.

No Use channels. It can float these pins.

Is it correct?

2. NC PINS: Pins(Pin11~14) internally not connected, do not float these pin

It needs to connect the external pull-down (PD) 10Kohm.

Is it correct?

Please check to reply us asap.

Thanks

B.R

Vincent