When Vdd = 0V, the voltage range that can be input to the C1 (SDA) and D1 (SCL) pins is -0.3V to Vdd+0.3V, or ±0.3V, is this correct? If I were to pull up with an external 3.3V, would the semiconductors be damaged?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When Vdd = 0V, the voltage range that can be input to the C1 (SDA) and D1 (SCL) pins is -0.3V to Vdd+0.3V, or ±0.3V, is this correct? If I were to pull up with an external 3.3V, would the semiconductors be damaged?
Hi Sawada,
This looks like a duplicate thread. Our team will support you on the other instance of this thread.
Thank you,
Jeff McPherson
Dear Jeff McPherson
Sorry about the duplicate thread. My mistake.
Thank you for your cooperation.
Best regards,