Part Number: ADC34J45
Was this test pattern discrepancy ever resolved? I am experiencing the same issue now 5 years after this original post and I don't see any resolution from the TI team.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Aaron,
Do you have the original post you can forward to me please and I can check into this?
Thanks,
Rob
Rob,
Here is the original post I am referencing: https://e2e.ti.com/support/data-converters-group/data-converters/f/data-converters-forum/653912/adc34j45-test-pattern-not-working-well
To add some context, I am now running into a similar finding. Here are the ADC34J45 test pattern discrepancies I've identified:
|
datasheet |
0 |
2399 |
8192 |
13984 |
16383 |
13984 |
8192 |
2399 |
|
actual |
2654 |
4276 |
8192 |
12107 |
13729 |
12107 |
8192 |
4276 |
Thanks,
Aaron
Aaron,
I think this is an error in the data sheet. We are checking with the design team regarding this. I did notice the deskew pattern was 0x2AAA but the 8-point sine wave I observed was different from what you are reporting. See attached captured results. The values I am seeing are 0, 12468, 10846, 12468, 0, 3915, 9633, 3915.
I also noticed in the data sheet the bits used for setting the test pattern modes are wrong in registers 0x0A and 0x0B.
Bits 7:4 of register 0x0A is used to set the pattern for CHA and bits 3:0 are used to set the pattern for CHB. Bits 7:4 of register 0x0B is used to set the pattern for CHC and bits 3:0 are used to set the pattern for CHD.
Regards,
Jim