Other Parts Discussed in Thread: ADS131M03
Hi Team,
Confirm one question: What is the input common-mode voltage when the ADC is a differential input? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kevin,
The ADS131M03 has an input range which is dependent on the PGA gain. Please see it in the following table on page 5 of the M02 datasheet.
For the Gain=1, 2 and 4, the inputs can be anywhere from (AGND-1.3)V to AVDD. For a higher gain between 8 and 128, the internal pre-charge buffer limits the top end range. In both conditions, the input signal can be lower than AGND because of a negative charge pump that was designed on the ADC. The device uses a different type of PGA implementation from other ADCs.
Regards,
Dale