Can't burn, please help see what caused it
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi user6350528,
We have no experience using the Xeltek programmer so it is difficult to say if the programming software is executing the correct commands for the MSC1211. Before attempting to flash a program to the device the MSC1211 must be placed into the Flash Programming Mode and then properly erased. If the contents cannot be erased, it is possible that the Hardware Configuration register (HCR0) has the security bit set to 0 which prevents the flash program memory from being erased, read or written to the device.
Most likely you will need to contact the vendor of the programmer to determine how to properly setup the programmer and how to erase the device.
Best regards,
Bob B