Thanks for your answers. Regarding answer #4 “The rails were swapped to make the PCB routing easier by removing crisscrossing that would have forced us to use multiple layers”, if the rails are swapped, wouldn’t it change the input signal polarity. I mean, if the input signal is at Max voltage and you swapped the rails, doesn’t the ADC will see it as Min voltage ?
Did you rely on AC signal only when you designed the eval board ?
Any layout recommendations for DC signal as well ? In case of DC - 250MHz signal, does crisscrossing is a must ?
Thanks,
Yuval