Hi Tom,
I am trying to scale ADS7881 outout but I couldn't manage to do it. I inputed 1.25 VDC to adjust R25 to mid scale but the code axis keep moving as I move R25. However, I adjusted R25 to set the DC line around 2045 code range. When I switched to sine wave, it was totally out of scope which can be seen in the 1st waveform shown in the figure given below.
http://i52.tinypic.com/2heftko.jpg
After that I adjusted R25 with sine wave, Y-axis shows code length from 0 to 4095, I tried to center the waveform aorund 2048, it has maximum value of 4095 but the waveform doesn't start from 0 which means it is not center around 2048 (0x800). It can be seen in the 2nd waveform given at the same link as above.
Can you please tell me if some thing is wrong ?
Thanks.