Other Parts Discussed in Thread: DAC53004, DAC63004,
Is it possible to switch the PowerDown modes (via PD0, PD1 and PD2 bits) independently per channel on the DAC5573 (or DAC63004/DAC53004)?
As example - Is it possible to get the following output voltages/High-Z's at the same time: Vout A to 2.5 V, Vout B to High-Z, Vout C to 2.5 V and Vout D to High-Z (with Vref = VDD = 5V)?
As I understand the register description in the datasheet on page 16 (DAC5573), this should work.
However, this is not explicitly mentioned in the description of the "Power-Down Modes" on page 23-24 (DAC5573).
Same question for DAC63004/DAC53004.