Hi team,
customer test the latency of ADS127L11 and found the result is different from the data in datasheet. Customer used synchronized mode and use 25MHz as Fclk, 400ksps as data rate, OSR=32, Sinc4. According to datasheet, the latency is10.63us. But customer test result is 11.4~11.7us. They use oscilloscope to test the time between rising edge of Start and first falling edge of DRDY.
Questions are:
1. How to calculate latency of every sinc filter?
2. Besides latency of sinc filter, is there any other factors will add latency ?
3. If customer give START like figure 8-25 in datasheet, are the first latency and the second latency same time?
4. Is 11.4us reasonable?
Thanks!
Rayna