HI!
I am planning to use DAC3283 for the below application and i have the below query,
Application:
DAC CLK: 4000MHz
Output Freq: 75 MHz
Query:
1)I have only CML clock outputs in my system with VOD=420mVpp (typ). Is there a way to interface CML clock to DACCLKP/N inputs of DAC3283?
2) will there be any degradation in phase noise of the outputs? If so, how much?
Thanks in-advance,
Deva