Other Parts Discussed in Thread: REG104
Hello,
When powering the MMB0 board provided with the ADS131E08EVM through the J2 power jack, I noticed that none of the voltage rail LEDs come on. Only the seven-segment display U10 lights up. I measured about 300mV at the 3.3V test points. The supply I am using is rated for 12V and 1A output, which should be within the required specifications.
Is there anything I am missing for proper functionality?