Hi again
Is it true that the full scale in single ended mode is only 13 bits instead of 14 bits wide? Is there a trick to get the full resolution?
Best regards
Timon Meier
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Timon,
Yes, you are correct. In this device when is set up in single-ended mode, you can only obtain 13-bits resolution. The ADS7871 input range is limited to 0-Vref in single ended mode so you can only obtain 13-bits because it converts using half the input range... If you are converting 8 single-ended inputs, there is not real trick to get the 14 bits of resolution.
If you have the ability to free some of the inputs and feed the negative inputs with a fixed voltage (for example using the voltage reference), then you could possibly set up the device in differential mode and run your single ended input using the +/-Vref range obtaining 14 bits.
Regards,
Luis.