Hi team,
When only one device is used and the daisy chain is not required, does the command, "Daisy-chain disable" need to be sent?
Regards,
Noriyuki Takahashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
When only one device is used and the daisy chain is not required, does the command, "Daisy-chain disable" need to be sent?
Regards,
Noriyuki Takahashi
Hi Takahashi-san,
No, it is not required. It looks like the daisy-chain disable setting determines if the data is clocked in on the 16th active clock edge, or on the rising edge of synch. This will determine which data is ignored if you happen to have more than 16 clocks in the write sequence.
Best,
Katlynne Jones
If only one device is used, no need to disable daisy-chain.