Hello,
The Datasheet gives the following formula for Analog input current calculation:
Is VIN the differential voltage between AIN_nX and AIN_nXG? Or is it the absolute voltage of each pin against AGND?
Regards
Sebastian
P.S.: When reworking the Datasheet, the unit of the formula could be rethought.
The result is in A.
Because of the value of RIN it is in the range of uA.