This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Following table 18 divide by 6, when attempting to use the ADC with an LMFS setting of 4211 we are getting an output that matches what we would expect with 4244. When setting LMFS we also get the behavior of 4244. This is present both when using the ramp test pattern in the DDC block and in normal oepration.
ADC Reg Dump:
Master Page Regs:
0x20: 0x0000
0x32: 0x0000
0x39: 0x0050
0x3c: 0x0000
0x3d: 0x0005
0x57: 0x0010
0x58: 0x0000
0x5a: 0x0000
ADC Page Regs:
0x3f: 0x0000
0x42: 0x0003
Offset Correction Page Regs: (Channel A Channel B)
0x68: 0x0042 0x0042
Digital Gain Page Regs: (Channel A Channel B)
0xa6: 0x0000 0x0000
Main Digital Page Regs: (Channel A Channel B)
0x00: 0x0000 0x0000
0xa2: 0x0008 0x0008
JESD Digital Page Regs: (Channel A Channel B)
0x01: 0x0080 0x0080
0x02: 0x0000 0x0000
0x03: 0x0002 0x0002
0x04: 0x0000 0x0000
0x06: 0x0000 0x0000
0x07: 0x001f 0x001f
0x16: 0x0070 0x0070
0x17: 0x0000 0x0000
0x32: 0x0000 0x0000
0x33: 0x0000 0x0000
0x34: 0x0000 0x0000
0x35: 0x0000 0x0000
0x36: 0x0040 0x0000
0x37: 0x0002 0x0002
0x3c: 0x0001 0x0000
0x3e: 0x0060 0x0060
Decimation Filter Page Regs: (Channel A Channel B)
0x00: 0x0001 0x0001
0x01: 0x0001 0x0001
0x02: 0x0000 0x0000
0x05: 0x0001 0x0001
0x06: 0x0000 0x0000
0x07: 0x0000 0x0000
0x08: 0x0000 0x0000
0x09: 0x0000 0x0000
0x0a: 0x0000 0x0000
0x0b: 0x0000 0x0000
0x0c: 0x0000 0x0000
0x0d: 0x0000 0x0000
0x0e: 0x0000 0x0000
0x0f: 0x0000 0x0000
0x10: 0x0000 0x0000
0x11: 0x0000 0x0000
0x14: 0x0000 0x0000
0x16: 0x0000 0x0000
0x1e: 0x0041 0x0041
0x1f: 0x0001 0x0001
0x33: 0x0000 0x0000
0x34: 0x0000 0x0000
0x35: 0x0000 0x0000
0x36: 0x0000 0x0000
0x37: 0x0004 0x0004
0x3a: 0x0000 0x0000
Power Detector Page Regs: (Channel A Channel B)
0x00: 0x0000 0x0000
0x01: 0x0010 0x0010
0x02: 0x0000 0x0000
0x03: 0x0000 0x0000
0x07: 0x00e6 0x00e6
0x08: 0x00cc 0x00cc
0x09: 0x00b3 0x00b3
0x0a: 0x0099 0x0099
0x0b: 0x0000 0x0000
0x0c: 0x0000 0x0000
0x0d: 0x0000 0x0000
0x0e: 0x0000 0x0000
0x0f: 0x0000 0x0000
0x10: 0x0000 0x0000
0x11: 0x0000 0x0000
0x12: 0x0000 0x0000
0x13: 0x0000 0x0000
0x16: 0x0000 0x0000
0x17: 0x0000 0x0000
0x18: 0x0000 0x0000
0x19: 0x0000 0x0000
0x1a: 0x0000 0x0000
0x1d: 0x0000 0x0000
0x1e: 0x0000 0x0000
0x20: 0x0000 0x0000
0x21: 0x0000 0x0000
0x22: 0x0000 0x0000
0x23: 0x0000 0x0000
0x24: 0x0000 0x0000
0x25: 0x0000 0x0000
0x27: 0x0000 0x0000
0x2b: 0x0000 0x0000
0x33: 0x0005 0x0005
0x34: 0x000d 0x000d
0x35: 0x000e 0x000e
0x36: 0x000e 0x000e
0x37: 0x0000 0x0000
0x38: 0x0000 0x0000
Other notes:
Previously we were using the ADC without decimation and LMFS of 8 2 8 20. Its possible we make a mistake when converting.
Doug,
I have setup the device for this mode again (using the GUI) and see the following as the ILAS configuration data. Does this match what you are seeing? I am still working on sample unpacking for this mode to see if the samples are showing as LMFS 4211 or 4244 with this config. I will share updates when I have them.
did: 0 | did: 0 | did: 0 | did: 0 |
bid: 0 | bid: 0 | bid: 0 | bid: 0 |
adjcnt: 0 | adjcnt: 0 | adjcnt: 0 | adjcnt: 0 |
lid: 3 | lid: 2 | lid: 1 | lid: 0 |
phadj: 0 | phadj: 0 | phadj: 0 | phadj: 0 |
adjdir: 0 | adjdir: 0 | adjdir: 0 | adjdir: 0 |
L: 3 | L: 3 | L: 3 | L: 3 |
scr: 0 | scr: 0 | scr: 0 | scr: 0 |
F: 0 | F: 0 | F: 0 | F: 0 |
K: 31 | K: 31 | K: 31 | K: 31 |
M: 1 | M: 1 | M: 1 | M: 1 |
N: 15 | N: 15 | N: 15 | N: 15 |
cs: 0 | cs: 0 | cs: 0 | cs: 0 |
Np: 15 | Np: 15 | Np: 15 | Np: 15 |
subclass: 1 | subclass: 1 | subclass: 1 | subclass: 1 |
S: 0 | S: 0 | S: 0 | S: 0 |
jesdv: 1 | jesdv: 1 | jesdv: 1 | jesdv: 1 |
cf: 0 | cf: 0 | cf: 0 | cf: 0 |
hd: 1 | hd: 1 | hd: 1 | hd: 1 |
reserved1: 0 | reserved1: 0 | reserved1: 0 | reserved1: 0 |
reserved2: 0 | reserved2: 0 | reserved2: 0 | reserved2: 0 |
fchk: 71 | fchk: 70 | fchk: 69 | fchk: 4 |
Regards, Chase
Sorry the table above is ultra hard to read. Below is a screenshot of excel. I'm not sure why my VIO captured the checksum correct for all lanes except for lane 0. If you calculate the checksum manually, it will be correct as value 68.
Hope to update again soon.
Regards, Chase
Hi Doug,
I have stayed later than usual tonight to check on this for you. I can confirm that the config that the gui makes is indeed LMFS4211. I have some lane mapping wrong in my FPGA firmware (DA1 swapped with DA2, and DB1 swapped with DB2), but I know this is 4421 for sure because this is an HD=1 mode (where samples are split across multiple lanes), and since there are only two lanes, whenever I place the ADC into ramp mode, the two bytes of the sample are swapped. Instead of the LSB incrementing, I am seeing bits 15:8 incrementing first and then bits 7:0 incrementing. This makes sense as if the lanes are swapped in 4211 mode, then the 8 MSB and the 8 LSB will be swapped per converter.
Here is the GUI configuration which I have used to test with the ADC. As it shows, I am using onboard clocking as this was the most convenient way for me to check this out. The sample rate of the ADC is 2457.6MSPS and in real ddc by 3 mode, LMFS4421, such that the output data rate = 819.2MSPS and serdes rate = 8192Mbps. Please use this to review the JESD configuration page for the converter. I have glanced at it and see that some values, such as JESD MODE 0-2 are showing a discrepancy between the GUI output (which works) and the datasheet recommendation (which seems to place the device into 4244 mode). Please try your config with these JESD settings.
RF45EVM_onboard_clk_2457p6M_LMFS4211.cfg
Regards, Chase