Other Parts Discussed in Thread: ADS8028, TINA-TI
I has to evaluate if the bipolar an unipolar AMC7836 input channels are correctly driven in my design (output resistance and GBW of the driver opamp, Rf and Cf correctly defined).
For that reason, I am looking on the AMC7836 documentation in order to establish the taq and Csh.
Taq can be established by means of the equation defined in the datasheet on page 77, while Csh is not declared or at least is 34pF for unipolar channels (input capacitance) and not declared for bipolar channels.
In addition, the bipolar channels of the AMC7836 have an internal resistor network used to scale the input signal (probably it is composed by two resistors with a value equal to 175k).
The value of Rmus is not defined.
The user guide of the AMC7836 Evaluation Module has inside the schematic a Csh for each analogue input of 470pF.
It is not available a PSPICE model of the ADC7836 or equivalent to be used to perform a simulation of the ADC Driver Circuit.
Have someone used this ADC?
How do you have established and verified that the driver circuit is correctly designed?
Thanks
Valerio