When connecting two TX7332 to a single AFE, what state must the second TX7332 be in?
Our board design works find with one TX7332 installed, but as soon as we solder in the 2nd TX7332, no pulse is measured on the output pins (of the 1st TX7332).
I assume it is a setting on the 2nd TX7332 which is at fault.
If it was still pulsing, but not visible on the AFE, I would suspect the TR Switch, but no pulse at all does not make sense to me.
Please can you assist.