TI_Genius Kirby stated that:
"The LVDS output runs off of the 1.8V drive. The rest of the part runs off of the 3.3V supply. The Vih and Voh are for the SPI and not for the LVDS output. Please see the LVDS Output table for the LVDS specification."
Kirby states that the Vih and Voh levels are for the SPI. The problem is that the Vih levels listed for SPI in table 6.6 correspond to a 3.3V interface but the Voh levels listed for SPI in table 6.6 correspond to 1.8V levels. So is it not correct for Kirby to state that the rest of the part runs off of the 3.3V supply?
I am asking if the SPI interface is 1.8V or 3.3V. The SPI input signals are listed with 3.3V levels but the SPI output signal is listed with a 1.8V level.
Note that Vih is for the SPI input signals SCLK, SEN, SDI and CLPIN, and that Voh is for the SPI output signal SDO.
Can Kirby or someone else please clarify?
Are the SPI input interfaces 3.3V signaling and the SPI output interfaces 1.8V signaling? It is fine if it is but please clarify that it is that way. It would just be nice if the datasheet stated that clearly.
Thank you,
scott