Other Parts Discussed in Thread: ADS1235
Hello,
I will be using the ADS124S06 in a wheatstone bridge application, and will be using manual AC excitation given that this ADC does not have the control logic integrated.
I have attached a simplified diagram - essentially my question is whether it is OK for the REFP/N pins to experience alternating polarity during the AC excitation sequence.
For example,
- While M1 & M4 are on:
- REFP0 = 3V (selected reference)
- REFN0 = 0V (selected reference)
- REFP1 = 0V
- REFN1 = 3V
- In this scenario REFP1 - REFN1 = negative 3V. Although this would not be the selected reference via SPI commands.
- While M3 & M2 are on:
- REFP0 = 0V
- REFN0 = 3V
- REFP1 = 3V (selected reference)
- REFN1 = 0V (selected reference)
- In this scenario REFP0 - REFN0 = negative 3V. Although this would not be the selected reference via SPI commands.
So, essentially the question is whether REFP/Nx can sustain a negative 3V voltage temporarily during the AC excitation phase? The TI example application note TIDUBL0A appears to do it this way, but I wanted to verify - specifically for ADS124S06
.