The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1235EVM: How to configure for connection to my processor instead of to usb

Part Number: ADS1235EVM
Other Parts Discussed in Thread: ADS1235

I want to connect the ads1235 on the evm to my processor evm to get a head start on s\w for a new board that has this adc and my processor. The processor EVM is connected on USB and has +5V available as an output.

I am clear on connecting the control lines thru J6. Same for the 3.3V. Not sure about the +5V. I think I need to to solder a jumper from J4-2 toJ4-3. But, do I also need to remove R94 and R95 (0 ohm)? And then, do I connect the 5V output from my processor evm board to J6 EXT_5V?