This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ti,
Currently, TI's DAC3XJ8X EVM is used to output a 49.9MHz Tone(Created by High Speed Data Converter Pro GUI), and then ADCxxQJxx00 is used for data capture.
The data transmission and capture board paired with two EVMs is both TSW14J57.
Under the default DAC configuration, the signals output by two channels (1 and 2, or 3 and 4) of the DAC are phase reversed. May I ask where to modify the configuration so that all DAC channels can output in-phase signals.
Please refer to the attachment for the DAC configuration page, ADC data acquisition interface, and oscilloscope display interface.
Thanks!
Thank you for your reply.
Also, I would like to ask another question. If using this EVM board to achieve DAC differential output, are the following modifications to the components feasible.
1. remove T1 and T2
2. connect the 4th pin of T1 to the 6th pin of T2 using a zero ohm resistor.
3. connect the 6th pin of T1 to the 4th pin of T2 using a zero ohm resistor.
Thanks!
Hi,
You will also need to connect 25ohm to ground (assuming your load is high Z). See below app note for detail: