Other Parts Discussed in Thread: DAC63204
Dear all,
I've got a project in which I used a DAC60508MRTER because I was under the impression that it would start-up mid-scale using the internal reference of 2.5V. I expected 1.25V on all outputs. But now, first time operating the actual hardware I realized, that it's 2.5V output all over the outputs. And after reading the datasheet more carefully (and here) I'm quite puzzled why would the gain register default to a gain of 2? I'm just starting to talk to the devices so I did not read-out the actual DAC register but I assume to find the mid-scale code in there anyways? ;-)
I think I have read majority of posts concerning this DAC-series here... Excuse my frank question: Am I missing a big point somewhere? Is is possible to start-up with 1.25V at all?
Thank you in advance,
Frank