Other Parts Discussed in Thread: ADS124S08
Hello,
I am currently using the TI Delta Sigma Evaluation Software to evaluate the ADS124S08. We are using a full wheatstone bridge made up of 4x strain gauges. The bridge resistance is 1000 ohms. I designed the circuit as per TIs A Basic Guide to Bridge Measurements (ti.com) page 51, 6.5 Four-Wire Resistive Bridge Measurement With a Ratiometric Reference and Current Excitation.
At the moment the evaluation software determines an ENOB of 12.5 bits which i think is quite low for this ADC. I was wondering if there was anyway to improve the performance or if you can spot anything glaringly wrong. .
Adc config:
20 sps
low latency filter
PGA gain of 128
IDAC 1 mA
IDAC current out of AIN3
AIN + = channel 8
AIN- = channel 9
When I run a data analysis at 1 V reference I get the following:
ENOB = 12.5 bits

Is there any way to improve this number? We would ideally like to measure down to at least 1 uV as that lets us resolve 1 uStrain.
I have set up the ADC eval kit as per below:
I have configured the IDAC on AIN3 to output 1 mA.
I've modified the evaluation kit slightly in order to include a bias resistor of 1.15K between Ref N0 and GND.
I am using AIN8 as positive input and AIN9 as negative.
I measure the correct 1.65 V common mode to both inputs.
Apologies for the poor diagram below but i hope it helps illustrate my circuit.

Any help with this one is appreciated.
Kind regards