Part Number: ADS1018
Other Parts Discussed in Thread: ADS1118, , ADS131M04, ADS131M03, ADS131E04, MSPM0G1107, ADS131M08, ADS131M06
Hi,
We need to Monitor the 3-phase Load Current using three Current Transformer(CT) for each phase. We need SPI communication based External ADC IC to read the CT secondary RMS Voltage. Microcontroller will communicate with ADC through SPI protocol to receive data.
CT Secondary(Out) Max Voltage will be 1Vrms, 50Hz. You can refer attached Waveform(Ch1: CT Out)
Kindly suggest us the suitable 12bit and 16bit ADC with 3 or 4 Channel.
Thanks and Regards,
Naveen K