This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm looking for an ADC to fit the following specifications.
Hi Edward Hunckler,
I know you said the ADS124S06 was more than you need, but is there any reason not to use this ADC other than it has more channels / features than is required? I assume you already have experience with this device from both a hardware perspective as well as code. If you switch to a new ADC you will need to write new code as well.
You could use the ADS124S06 and use the REFOUT feature to bias your RTD using voltage excitation. This way, your signal and your reference (the internal reference) are ratiometric, which should yields the best results. Note that the ADS1246 does not offer this feature as it does not have an internal reference.
Also, the ADS1246 cannot support a VREF that is the same as the supply, see the image below. Note that VREF (max) must be AVDD-AVSS-1 V, or 2.3V in your case. There are some simple ways to get around this, but I just wanted to point out that the circuit as you have drawn will not work.
-Bryan