This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC81408: Data converters forum

Part Number: DAC81408

Dear TI team

I have three questions for this DAC IC.

1. Is it correct that the power down mode function works at the timing of [power off → power on], and the glitch is 0.3V at the maximum?
Or is there a difference between power down mode and power off?


2. What is the voltage level the glitch of power on → power off?


3. Is there no sequence rule for power off as well?
Also, what is the recommended sequence to reduce the glitch?

Best regards,

T.C.

  • Hi T.C.,

    Sanjay will review your questions and provide a response soon. 

    Best,

    Katlynne Jones

  • Hi T.C.,


    Please check my response below for each line item -

    1. Is it correct that the power down mode function works at the timing of [power off → power on], and the glitch is 0.3V at the maximum?
    Or is there a difference between power down mode and power off?

     - Yes, the power down mode function works at the timing of [power off → power on], and the glitch is 0.3V at the maximum. This is to check the DAC output enable glitch magnitude. 

    2. What is the voltage level the glitch of power on → power off?

     - Currently there is no such data sheet specification available for power on → power off but it should not be much different from the power off → power on glitch magnitude. 


    3. Is there no sequence rule for power off as well?
    Also, what is the recommended sequence to reduce the glitch?

    - Yes, there is no sequence rule for power off. Recommended sequence to reduce the glitch is first power on VAA/VDD/VIO and then VCC/VSS, REFIO should come up at the end. 

    Thanks,

    Sanjay