This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7049-Q1: 4-wire SPI

Part Number: ADS7049-Q1

Tool/software:

Customer is looking for the below SPEC ADC:

12BIT ADC、1MSPS、4-wire SPI, Cost effective.

ADS7049 could meet the spec but it's 3-wire SPI that is not meeting customer's SPI interface. Please help to recommend a similar one with 4-wire SPI interface. thanks. 

Regards

Brian

  • Hi Brian,

    Why do you need 4-wire SPI?  The typical lines are SCLK, /CS, SDO and SDI.  SDI is only used with multi-channel based parts or devices that have a configuration register of some sorts.  The ADS7049 has no need for a DATA INPUT, so there is only a 3-wire SPI interface.  I don't understand why this would be an issue for you.  Can you clarify and provide application details?  Why do you need SDI?

  • Hello Tom,

    Long time no see. Hope you're doing well.

    Since Encoder is using ASIC to do the magnetic signal converter and other functions, ASIC is only supporting 4-wire SPI interface. is that making sense? 

    Regards

    Brian

  • Doing well Brian,

    The ADS7049-Q1 has no need for SDI.  Since there is no need for SDI, you only need 3-wires for control.  What is the ASIC trying to write too?  Send me a note with more details please.

  • Hello Tom,

    Customer mentioned in the Encoder system, there're two devices using 4-wire SPI comm with ASIC.

    One is angle sensor MT6835, the other one is ADS794x(for example). The SDI function is needed to handshaking which data in the Sensor or ADC is needed for ASIC. Is it making sense?  

    Is there low-cost 4-wire ADC with the sample requirements you recommended?

    ASIC SPI pinout:

    Angle Sensor: 4-Wire SPI

    Regards

    Brian

  • Nope - still don't see the need.  Please set up a call and we can discuss further.