This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4900: Device configuration constraints for 1 channel operation

Part Number: AFE4900

Tool/software:

Hello,

Note: these settings can be saved and entered into the AFE4900 EVM as a xxx.cfg file.

I am hoping that someone who has ACTUALLY USED the AFE4900 responds to this post.

My configuration is as follows:
LED1 - green
LED2 - red
LED3 - IR
LED4 - green2

What I attempted to configure was

LED1 pulse - sample - convert

and ambient sample - convert

and save to FIFO.

but it appears that does not work.

For some reason it wants

LED2 ( pulse - sample - convert )
LED1 ( pulse - sample - convert )

so I set LED2 drive current to 0 milliamps as a work around.

This is a power constrained device - I assume extra phases are not good for
minimum power consumption.

I created a configuration like this for the AFE4900 EVM

it also mis-behaves - It is attached.

Can someone please explain to me the underlying assumption
about the phase order and what is needed ?

The datasheet says that setting a count register to >PRPCOUNT should disable it - but there is
something else going on in the LED1 only configuration.

The timing calculator.xls spreadsheet only works for all 4 phases - anything else gives an error.bad_config2.cfg
The AFE4900 EVM is also unhappy with only 1 LED1 phase.

I can successfully gather data, but I have used other PPG IC's from other manufacturers
and had no limitations such as this.

I also plan on using LED2 and LED3 as a sampling pair for SPO2.

If someone had a RTL description or VHDL of the part I would be able to understand it's timing
sequencing limitations.

Looking forward to hearing from you.

JBS

  • I have resoled the problem.

    So that others are not confused by incorrect results:

    1) the AFE4900 EVM is not compatible with all the different timing configurations that the device is capable of.

    2) the AFE4900_Timing_Calculator_V3 timing spreadsheet is also not compatible with all the different timing configurations that the device is capable of.

    3) the Table 30. section 8.3.9.1 on page 42 is incorrect.

    4) Turns out that there is a second table - the correct table 138  is on page 131.

    JBS