Tool/software:
Hello,
was are using TSC2008TRGVRQ1 and our prototypes worked pretty well. I am now seeing a lot of noise on the IRQ line and it is locking up the microprocessor. We found the cause as our speaker in the front panel that shares the touch screen. Moreover, the PWM driver of the speaker goes via a pi-filter which connects to the chassis.
Overall, a combination is causing it.
I read in the datasheet that we can add capacitors to the 4 pins. What value do you recommend as a start? Please see my circuit below.