Tool/software:
We are using ADS1014BQDGSRQ1 now.
Here are our settings: VDD=5V, INP=1.5V~3.6V, INN=GND, FSR=±4.096 V
In this case, the LSB=2mV.
We measured that there is a ripple of about 25mV in INP. Will this have any effect on the LSB and output?
If we want to verify the accuracy of the output, what validations do we need to do? Which of these are for the input?