This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We don't provide kernel drivers for our devices. Only the EVM GUI software is available.
Regards,
Geoff
Hi Praven,
The SPI information starts on page 54 of the ADC3444 datasheet and goes through the initialization and programming of the device. Below is the datasheet link.
https://www.ti.com/lit/gpn/adc3444
Regards,
Geoff
Hi Pravin,
Unfortunately no, the datasheet acts as the reference.
Thanks, Chase
Hi Pravin,
I’m not exactly sure what you mean by managed or unmanaged. Can you elaborate?
This device will work without requiring any register writes after power up. These are features you can turn on or off after power up. Each power cycle, the register information is reset to the default value shown in the datasheet.
Thanks, Chase
Hi Chase,
Managed and unmanaged means I have asked if this device will work with driver support only or if it will work without driver support also.
According to your statement (This device will work without requiring any register writes after power up), I think there is no need for driver support on the software side. Is it?
Hi Pravin,
Given these features are optional and there is no driver for this device already existing, then no, a driver is not required. However, I would advise connecting the SPI interface in your design regardless so you can design a spi controller driver later on if needed.
Thanks, Chase