This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC39RF12: Output signal sync with the phase

Part Number: DAC39RF12

Tool/software:

Hello team,

My customer wants to align the phase of this DAC with external sampling circuit.
Customer just need this DAC to output short pulse, which is aligned with the phase of the output.

Please refer to my drawing below.

Would it be possible to achieve it by SYNC pin of DAC39RF12?

Best Regards,
Kei Kuwahara

  • Hello, 

    The SYNC pin on the DAC is an output used for the 8b10b mode of operation of the JESD204 serial interface. There is no way to use the SYNC output pin in relation to the frequency word of the NCO. 

    Regards, 

    Matt