This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
The supplied 20-bit_Configs.txt file defines SPI writes for configuration. The question is if ther is a way to load that file through the ADC35xx_EVM_GUI? The program has a Python script load facility, but I'm not sure what sort of script can be loaded and whether it will use the on-board FTDI chip to send the USB writes over the ADC's SPI interface. Any comment? Or is there a stand-alone simple register read/write utility to allow reading and writing the the ADC on the eval board over USB?
Hi Maxim,
I answered your question in your other related E2E post. Therefor I will be closing this one.
Best regards,
Drew