Part Number: ADS9219EVM
Other Parts Discussed in Thread: TSWDC155EVM, ADS9219
Tool/software:
I recently purchased a ADS9219EVM and TSWDC155EVM.
After connecting the TSWDC155EVM to +5V and USB and starting up the GUI only LEDs D16, D17, and D20 turn on.
All the LEDs associated with the various lower voltages do not turn on.
I followed the instructions in "User's Guide TSWDC155EVM" (SLAU870 - March 2022), where in section 5.1 EVM Powerup, it states that 8 LEDs should start glowing.
Note that the pictures of the EVM in these instructions do not match my module (see attached image).
I assume the other errors I get through the GUI are related to the apparent power on problem, missing low voltages: 2.5V, 1.8V, 1.35V, 1.2V (no LEDs on and the measure zero on test points).
I have also attached the GUI log.
Does anyone have ideas regarding bringing up this eval system?
Sven.

Log -------------------------------------------------------
ADS9219: selected
18b capture
Programming FX3...
FX3 already programmed
disconnect and connect the cable again to Program the FX3
#Error: 'NoneType' object has no attribute 'DownloadFw'
# "", line 41, in
# File "", line 25, in downloadFW
# AttributeError: 'NoneType' object has no attribute 'DownloadFw'
#
#
#================ ERRORS:1, WARNINGS:2 ================#
Pheripheral controller initialization done
Click on Program FPGA
Loading...
USb Device with VID1105 and PID 37185 not found.
USB Device with VID1105 and PID 37185 not found.
USb Device with VID1105 and PID 37185 not found.
USB Device with VID1105 and PID 37185 not found.
USb Device with VID1105 and PID 37185 not found.
USB Device with VID1105 and PID 37185 not found.
Powering ON Sparrow
#Error: 'SparrowController' object has no attribute 'controlep'
# "", line 17, in
# File "proj_lib\interfaces\mSparrowRegProgrammer_arevo.py", line 331, in sparrow_pwr_on
# File "proj_lib\interfaces\mSparrowRegProgrammer_arevo.py", line 318, in sparrow_pwr_on
# File "proj_lib\interfaces\mSparrowRegProgrammer_arevo.py", line 134, in fx3_gpio_write
# AttributeError: 'SparrowController' object has no attribute 'controlep'
#
#
#================ ERRORS:8, WARNINGS:0 ================#
DUMMY2 - No Capture Device defined
DUMMY2 - Reset property was not found
ADS92xx REGISTER MAP - No Capture Device defined
ADS92xx REGISTER MAP - Reset property was not found
devInit ran successfully and DML loaded!!!
#================ ERRORS:0, WARNINGS:5 ================#
Click on Initialize ADS98xx
ADS92xx REGISTER MAP - Device registers reset.
ADS92xx REGISTER MAP - Reset property was not found. Use setResetProperty() to fix this.