Part Number: ADS1230
Other Parts Discussed in Thread: ADS1232REF, ADS1231REF, ADS1232
Tool/software:
Hi, I need the EVM board or reference design for ADS1230 and also the sample code.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1230
Other Parts Discussed in Thread: ADS1232REF, ADS1231REF, ADS1232
Tool/software:
Hi, I need the EVM board or reference design for ADS1230 and also the sample code.
Hello Rohit,
We no longer offer the ADS1230REF boards. As an alternative, you can use either the ADS1232REF (24b version with 2 input channels and multiple gain options) or the ADS1231REF (24b, single gain of 128, includes low side bridge switch).
We also do not have example code available for these devices, but the interface is a very simple 2-wire interface that is compatible with SPI or can be bit-banged on GPIO.
Please refer to the below post for further details:
There is also 3rd party example code on GitHub for the ADS1232 that may be helpful as a starting point for ADS1230 code development.
Regards,
Keith Nicholas
Precision ADC Applications