Hello,
I was wondering if TI has a quad DAC exactly like the TLC7226 (PDIP) but with a higher resolution for example 10 bit instead of 8?
Here are some specs:
1) output dac voltage: 2 to 3.3 VDC
2) PDIP packaging
3) 10 or 12 bits resolution
4) Parallel interface
5) Selectable 1 Dac one output at a time
6) Quad dac
7) Retains voltage at Dac output when other channels are selected
I was looking at the DAC7625... but its max output seems to be 2.5VDC ????
I was also looking at the DAC7724... would this be the right fit?
all feedback appreciated!
thanks