Dear TI team,
We need your help on the following. In our design, are planning to use LM4140 to drive the reference pins for ADS1255 and wanted some help from TI to identify the right approach to do so.
We are wondering - (a) if we could use LM4140 to directly drive the reference
OR
(b) should we consider buffering it (using OPA350) on lines of what is described in the TI EVM schematics and datasheet? TI EVM uses REF5025
On (a), if we use LM4140 to directly driving the ADS1255 reference pins, the output load current on the regulator should be around 135uA (input impedance @ 30KSPS is 18.5KOhm) which LM4140 should be able to source without losing regulation. I have compared REF5025 datasheet to LM4140 and see that REF5025 also "seems" capable to drive the reference pins of ADS1255 directly. But the example shown specifically uses an op-amp (OPA350) to buffer the same and does not connect REF5025 directly to the reference pins.
Could you please explain if an op-amp is required to drive the reference pins or is it safe to drive the ADS1255 reference pins directly with an LM4140? A quick response will be greatly appreciated.
With Best Regards,
Sridhar