Hello,
I planned to make use of the PWM signal generated by the Sigma-Delta Modulator AMC1203 in order to drive a H-Bridge with Gate Driver ICs. According to datasheet of AMC1203, the output rate of AMC1203 is 10MHz. However, the response speed of Gate Driver ICs and MOSFETs in H-Bridge are not fast enough for a 10-MHz PWM signal.
So, are there any methods that can slow down the PWM signal, which is produced by AMC1203, to about 200KHz? If it is impossible to do so, are there any Gate Driver ICs and MOSFETs that fast enough to respond the 10-MHz signal?
Thank you for your help.